Device support {#topic_gfn_ldj_lyb}
The device folder contains the whole software enablement available for the specific System-on-Chip (SoC) subfamily. This folder includes clock-specific implementation, device register header files, device register feature header files, CMSIS derived device SVD, and the system configuration source files. Included with the standard SoC support are folders containing peripheral drivers, toolchain support, and a standard debug console.
The device-specific header files provide a direct access to the microcontroller peripheral registers. The device header file provides an overall SoC memory mapped register definition. The folder also includes the feature header file for each peripheral on the microcontroller.
The toolchain folder contains the startup code and linker files for each supported toolchain. The startup code is a CMSIS-compliant startup code that efficiently transfers the code execution to the main()
function.
Board support {#topic_iz1_4dj_lyb}
The boards folder provides the board-specific demo applications, driver examples, wireless connectivity examples, and RTOS examples.
Parent topic:Device support
Demo applications and other examples {#topic_kq5_pdj_lyb}
The demo applications demonstrate the usage of the peripheral drivers to achieve a system level solution. Each demo application contains a readme
file that describes the operation of the demo and required setup steps.
The driver examples demonstrate the capabilities of the peripheral drivers. Each example implements a common use case to help demonstrate the driver functionality.
Parent topic:Device support
Parent topic:MCUXpresso SDK release package