Middleware {#topic_z1q_f2j_lyb}

RTOS {#topic_vhw_h2j_lyb}

The MCUXpresso SDK is integrated with the FreeRTOS OS.

Parent topic:Middleware

Wireless connectivity middleware summary {#wireless_connectivity_middleware_summary}

Bluetooth LE host stack and applications {#bluetooth_le_host_stack_and_applications}

The Bluetooth LE Host Stack component provides an implementation for a Bluetooth 5.3 mandatory and some optional, proprietary, and experimental features. The Bluetooth LE Host Stack component provides application examples, services, and profiles.

Main features supported:

  • Automotive Compliance

  • MISRA Compliance

  • HIS CCM <= 20

  • Advanced Secure Mode

  • Enhanced ATT

  • GATT Caching

  • Bluetooth LE Host GCC Libraries

  • Bluetooth LE Host IAR Libraries

  • Bluetooth LE Host Peripheral Libraries

  • Bluetooth LE Central Libraries

  • Bluetooth LE Host Full Host Features Libraries

  • Bluetooth LE Host Optional Features Libraries

  • Bluetooth LE Host Mandatory Features Libraries

  • Bare-metal and FreeRTOS Support

  • Bluetooth LE Privacy Support

  • NCP Mode - FSCI Application

  • CCC Sample Applications - Controlled Access

  • Enhanced Notifications

  • Dynamic Database

  • OTA Support - Sample Applications

  • Decision based Advertising Filtering (DBAF) - Experimental feature

  • Advertising Coding Selection (ACS) - Experimental feature

  • Periodic Advertising with Responses (PAwR) - Experimental feature

  • Encrypted Advertising Data (EAD) - Experimental feature

    Note: For evaluating experimental features, replace the Bluetooth LE Host default example projects libraries with the libraries from the SDK folder ..\middleware\wireless\bluetooth\host\lib_exp and enable the features in the application. The Radio Subsystem (NBU) Firmware with experimental features is required.

Parent topic:Wireless connectivity middleware summary

Bluetooth LE controller {#bluetooth_le_controller}

  • Main features supported:

    • Peripheral Role

    • Central Role

    • Multiple PHYs (1 Mbps, 2 Mbps, Coded PHY)

    • Asymmetric Connections

    • Public/Random/Static Addresses

    • Network/Device Privacy Modes

    • Extended Advertising

    • Extended Scanning

    • Passive/Active Scanning

    • LE Encryption

    • LE Ping Procedure

    • HCI Test Interface

    • UART Test Interface

    • Randomized Advertising Channel Indexing

    • Sleep Clock Accuracy Update - Mechanism

    • ADI Field in Scan Response Data

    • HCI Support for Debug Keys in LE - Secure Connections

  • Main capabilities supported:

    • Simultaneous scanning 1 Mbps and Long Range

    • Scanning and advertising in parallel

    • 24 connections as central role

    • 24 connections as peripheral role

    • Any combination of central and peripheral roles (24 connections maximum)

    • Eight connections with 7.5 ms connection interval

    • Two advertising sets in parallel

    • 26 Accept List entries

    • 36 Resolvable Private Address (RPA) entries

    • Up to six Chain Packets per Extended Advertising set

    • Enhanced Notification on end of - Scanning/Advertising/Connection events

    • Connection event counter associated to Bluetooth LE packet reception

    • Timestamp associated to Bluetooth LE packet reception

    • RF channel info associated to Bluetooth LE packet reception

    • NXP proprietary Bluetooth LE Handover feature

    • Support for experimental features Advertising Coding Selection, Periodic Advertising with Responses (PAwR), and Decision Based Advertising Filtering (DBAF)

Note: Project configurations that require usage of the Bluetooth LE controller including all Bluetooth LE examples require the Radio Subsystem (NBU) Firmware to be re-programmed with the firmware provided in the SDK under middleware\wireless\ble_controller\bin. See the EVK Quick Start Guide and Secure Provisioning SDK (SPSDK) documentation for NBU programming steps.

Note: Project configuration enabling Experimental features requires the Radio Subsystem (NBU) Firmware to be reprogrammed with the firmware provided in the SDK under \middleware\wireless\ble_controller\bin\experimental\. For NBU programming steps, see the EVK Quick Start Guide and Secure Provisioning SDK (SPSDK) documentation.

Parent topic:Wireless connectivity middleware summary

XCVR {#xcvr}

The XCVR component provides a base Transceiver Driver for the 2.4 GHz narrowband radio.

Parent topic:Wireless connectivity middleware summary

Low-power reference design applications (central and peripheral)

The Low-Power Reference Design Applications provide reference design source code and projects showcasing how to implement optimized low power functionality based on a Bluetooth LE application. For additional details, see the readme.md.

Parent topic: Wireless connectivity middleware summary

Connectivity framework {#connectivity_framework}

The Connectivity Framework is a software component that provides hardware abstraction modules to the upper layer connectivity stacks and components. It also provides a list of services and APIs, such as, Low power, Over the Air (OTA) Firmware update, File System, Security, Sensors, Serial Connectivity Interface (FSCI), and others. The Connectivity Framework modules are located in the middleware\wireless\framework SDK folder.

Parent topic:Wireless connectivity middleware summary

Parent topic:Middleware

Wireless connectivity middleware overview {#topic_vnq_cgb_zwb}

Component versions:

Wireless connectivity component

Version

middleware/​wireless/​bluetooth

1.10.3

middleware/​wireless/​ble_​controller

1.9.20.0

middleware/​wireless/​xcvr

​2.​1.4

middleware/​wireless/​genfsk

4.0.22

middleware/wireless/framework

7.0.1b

The following connectivity-supporting documentation is included with this release:

  • Bluetooth Low Energy Quick Start Guide

  • Bluetooth Low Energy Demo Applications User’s Guide

  • Bluetooth Low Energy Application Developer’s Guide

  • Bluetooth Low Energy Host Stack API Reference Manual

  • Bluetooth Low Energy Host Stack FSCI Application Programming

  • Bluetooth Low Energy Host Stack FSCI Reference Manual

  • Bluetooth Low Energy CCC Digital Key Application Note

  • Generic FSK Link Layer Quick Start Guide

  • Generic FSK Link Layer API Reference Manual

  • Connectivity Framework Reference Manual

  • Connectivity Framework API Documentation

  • Low Power Connectivity Reference Design User’s Guide

Parent topic:Middleware

Other middleware {#other_middleware}

Optional middleware packages can be included in the release based on the user selection. See <install_dir>/SW-Content-Register.txt for a list of components and associated licenses.

Parent topic:Middleware

Parent topic:MCUXpresso SDK release package