Run an example application

To download and run the application, perform these steps:

  1. Reference the table in Default debug interfaces to determine the debug interface that comes loaded on your specific hardware platform.

  2. Connect the development platform to your PC via USB cable.

  3. Open the terminal application on the PC, such as PuTTY or TeraTerm, and connect to the debug serial port number (to determine the COM port number, see How to determine COM port). Configure the terminal with these settings:

    1. 115200 or 9600 baud rate, depending on your board (reference BOARD_DEBUG_UART_BAUDRATE variable in the board.h file)

    2. No parity

    3. 8 data bits

    4. 1 stop bit |

|

  1. To debug the application, click load (or press the F8 key). Then, click the Start/Stop Debug Session button.

    Note: Make sure that the board is set to FlexSPI flash boot mode (U38 all off) before using Keil debug.

    |

|

  1. Run the code by clicking Run to start the application.

    |

|

The `hello_world` application is now running and a banner is displayed on the terminal. If this is not true, check your terminal settings and connections.

|![](../images/hello_world_lowercase.png "Text display of the hello_world
										demo")

|

Parent topic:Run a demo using Keil MDK/μVision