Hardware requirements

  • Mini/micro USB cable

  • EVKB-IMXRT1050 board

  • Personal Computer

  • RK043FN02H-CT or RK043FN66HS-CT6 LCD board (RK043FN02H-CT and RK043FN66HS-CT6 are compatible)

  • MT9M114 module This example supports OV7725 too, if OV7725 is used, then MT9M114 is not necessary.

Board settings

  1. Connect the RK043FN02H-CT or RK043FN66HS-CT6 to board.

  2. Connect the MT9M114 or OV7725 camera module.

Prepare the Demo

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Note: If OV7725 is used, change the macro DEMO_CAMERA to DEMO_CAMERA_OV7725 in camera_support.h

Running the demo

When the demo runs successfully, the camera received pictures are shown in the LCD.