Hardware requirements

  • Micro USB cable

  • MIMXRT1060-EVKB board

  • JLink Plus

  • 5V power supply

  • Personal Computer

  • RK043FN02H-CT or RK043FN66HS-CT6 LCD board (RK043FN02H-CT and RK043FN66HS-CT6 are compatible)

  • SD card

Board settings

  1. Connect the RK043FN02H-CT or RK043FN66HS-CT6 to board.

  2. Unzip the pics.zip, place the jpg pictures to the SD card.

  3. Insert the SDCARD into card slot.

  4. Make sure resistors R368/R347/R349/R365/R363 are removed.

Prepare the Demo

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Insert SD card to card slot

  4. Download the program to the target board.

  5. Launch the debugger in your IDE to begin running the demo.

Running the demo

If this example runs correctly, pictures are shown in the lcd panel one by one.