Hardware requirements
Mini/micro USB cable
MIMXRT1170-EVKB board
Personal Computer
RK055MHD091 panel or RK055AHD091 panel or RK055IQH091 panel
Board settings
Connect the panel to J48 Connect 5V power to J43, set J38 to 1-2
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Build the project, the project uses RK055MHD091 by default, to use other panels, change #define DEMO_PANEL 2 to #define DEMO_PANEL 0 or #define DEMO_PANEL 1 or #define USE_MIPI_PANEL 3 in mcux_config.h Which number represent which panel can be found in display_support.h.
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs, you can see a polygon vector graphic with high render quality on a black buffer. The polygon is drawn on a temporary buffer, then it is rendered on the render target using a blit operation.