Hardware requirements

  • Mini/micro USB cable

  • Target microcontroller board

  • Personal Computer

  • FreeMASTER 2.5 or later installed on PC

Board settings

No special settings are required. The demo communicates by uploading and downloading communication frames directly to/from the microcontroller RAM buffer using the Debug USB port. Standard debugger must not be active during the FreeMASTER communication.

Prepare the demo

  1. Connect a USB cable between the host PC and the Debug USB port on the target board.

  2. Use one of the flash-based build targets.

  3. Compile and download the program to the target microcontroller.

  4. Run and resume application execution when debugger stops in the main() function.

Disconnect the debugger

  1. Terminate the debugger session to release the JTAG interface for FreeMASTER use.

  2. Reset the target board to make sure it runs after detaching the debugger.

Connect with FreeMASTER

  1. Run FreeMASTER, use the Connection Wizard or open Project Options.

  2. Select communication using the FreeMASTER Packet Driven BDM Communication (PD-BDM) plug-in.

  3. Configure the PD-BDM plug-in:

    • Use the same “underlying” BDM/JTAG interface as used in debugger (typically CMSIS-DAP).

    • Configure this BDM/JTAG interface and test its connection.

    • Specify or search for a RAM address of the “_pdbdm” communication buffer.

    • Test connection and close the configuration dialog.

  4. Start communication, FreeMASTER loads the initial TSA Active Content links in the Welcome page.

  5. Click the “FreeMASTER Demonstration Project (embedded in device)” in the Welcome page.

  6. The demo is now running, you should be able to watch variable values and graphs.

More information

Read more information about FreeMASTER tool at http://www.nxp.com/freemaster. Feel free to ask questions and report issues at FreeMASTER’s community page at https://community.nxp.com/community/freemaster