Hardware requirements
Micro USB cable
MIMXRT1040-EVK board
RK043FN02H-CT or RK043FN66HS-CT6 LCD board
Personal Computer
Board settings
Connect the RK043FN02H-CT or RK043FN66HS-CT6 to board.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Build the project, the project uses RK043FN66HS-CT6 by default, to use other panels, change #define DEMO_PANEL DEMO_PANEL_RK043FN66HS to #define DEMO_PANEL DEMO_PANEL_RK043FN02H in emwin_support.h
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
PXP command queue example start...