Hardware requirements
Mini/micro USB cable
EVK-MIMXRT1064 board
Personal Computer
Headphone(OMTP standard)
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Insert the headphones into the headphone jack on EVK-MIMXRT1064 board (J12).
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
Note: This demo outputs 215HZ sine wave audio signal. When the demo runs successfully, you can hear the tone and the log would be seen on the OpenSDA terminal like:
SAI functional interrupt example started!
SAI functional interrupt example finished!