Hardware requirements
Micro USB cable
EVK-MIMXRT595 board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J40) on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
TRNG Peripheral Driver Example
Generate 10 random numbers:
Random[0] = 0x201FEB53
Random[1] = 0x85A32C28
Random[2] = 0xDC66342C
Random[3] = 0xFD43ACFF
Random[4] = 0x1CD53C0
Random[5] = 0xB27EDBEB
Random[6] = 0x32AB81D5
Random[7] = 0x6AA5B70F
Random[8] = 0x81C41286
Random[9] = 0xC9620BD8
Press any key to continue...