Hardware requirements
Micro USB cable
FRDM-K32L3A6 board
Personal Computer
micro SD card
Board settings
1.Please insert the SDCARD into card slot(J9) 2.Make sure R153. R154, R156, R157 is switch to 1-2. Note: Due to FRDM board do not provide 1.8V IO voltage for SD part, so cannot switch to DDR50 mode. And the CARD detect PIN level is high when card is inserted.
Prepare the Demo
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the demo runs successfully, the log would be seen on the terminal like:
Card size xxxxx bytes
Working condition:
Voltage : xxxV
Timing mode: xxx
Freq : xxx HZ
Read/Write/Erase the card continuously until encounter error......
Write/read one data block......
Compare the read/write content......
The read/write content is consistent.
Write/read multiple data blocks......
Compare the read/write content......
The read/write content is consistent.
Erase multiple data blocks......
Input 'q' to quit read/write/erase process.
Input other char to read/write/erase data blocks again.