Hardware requirements
Type-C USB cable
FRDM-MCXA153 board
Personal Computer
Board settings
ADC CH0A input signal J4-8(PIO2_0).
Prepare the Demo
Connect a Type-C USB cable between the host PC and the MCU-Link port(J15) on the target board.
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
LPADC Interrupt Example
ADC Full Range: 65536
Please press any key to get user channel's ADC value.
ADC value: 35852
ADC interrupt count: 1
ADC value: 35586
ADC interrupt count: 2