Hardware requirements

  • Mini USB cable

  • FRDM-MCXC242 board

  • Personal Computer

Board settings

SPI one board:

  • Transfer data from instance0 to instance 1 of SPI interface, SPI0 pins are connected with SPI1 pins of board

INSTANCE0        CONNECTS TO         INSTANCE1
Pin Name   Board Location     Pin Name  Board Location
MOSI       J2 pin 8           MOSI      J2 pin 18
MISO       J2 pin 10          MISO      J2 pin 20
SCK        J2 pin 12          SCK       J1 pin 11
PCS0       J2 pin 6           PCS0      J1 pin 9

Prepare the Demo

  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Running the demo

When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

SPI one board interrupt example started!

SPI transfer finished!