Hardware requirements
Type-C USB cable
FRDM-MCXN947 board
Personal Computer
Board settings
Prepare the Demo
Connect a type-c USB cable between the PC host and the MCU-Link USB port (J17) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
Flash Hiding example...
FLASH_Init PASSED
FFR_Init PASSED
Erasing FLASH sectors, address: 10000, size:8000
flash_page_erase PASSED
Programming FLASH, address: 10000, size: 1000
flash_page_program PASSED
FLASH hiding no enabled and read PASSED!
MBCAddr = 0
MBCAddr = 500
FLASH hiding enabled and read limit PASSED
flash hiding test erase and program PASSED
CDPA example...
FLASH_Init PASSED
FFR_Init PASSED
Before enabling the CDPA, call flash_erase API and flash_program API ...
Erasing FLASH sectors, address: 18000, size:8000
flash_page_erase PASSED
Programming FLASH, address: 18000, size: 1000
CDPA no enabled and flash_program PASSED
CDPABlock = 0
CDPABlock = 4000
CDPA enabled and read test PASSED
CDPA test erase and program PASSED