Hardware requirements

  • Mini/micro USB cable

  • Personal Computer

  • FreeMASTER 3.1.2 with TCP/UDP communication plug-in installed

Board settings

Connect JP13 2-3 pin. Populate R274 to sync reference clock.

Make sure to connect the Ethernet cable to the board and interconnect it with the PC using a network switch. The demo uses static IP address or an address obtained from DHCP. Refer to network.c (EXAMPLE_USE_DHCP) file for more details about default IP address.

Prepare the demo

  1. Interconnect the board with a switch and the host computer.

  2. Compile and download the program to the target microcontroller.

  3. Run and resume application execution when debugger stops in the main() function.

Connect with FreeMASTER

  1. Run FreeMASTER, use the Connection Wizard or open Project Options.

  2. Select network communication and configure the plug-in for TCP or UDP protocol with the port that matches the settings in the freemaster_cfg.h.

  3. Start communication, FreeMASTER loads the initial TSA Active Content links in the Welcome page.

  4. Click the “FreeMASTER Demonstration Project (embedded in device)” in the Welcome page.

  5. The demo is now running, you should be able to watch variable values and graphs.

More information

Read more information about FreeMASTER tool at http://www.nxp.com/freemaster. Feel free to ask questions and report issues at FreeMASTER’s community page at https://community.nxp.com/community/freemaster