Hardware requirements
Mini/micro USB cable
KW45B41Z-LOC Board
Personal Computer
Board settings
Prepare the Demo
Connect a USB cable between the host PC and the LOC board J3.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the demo in the terminal window:
Tickless Demo example
Press or turn on SW3 to wake up the CPU
Tick count :
0
5000
CPU woken up by external interrupt
10000