Hardware requirements
Mini USB cable
LPCXpresso54S018M board
Personal Computer
Board settings
Insert the card into the card slot
Prepare the Example
Connect a mini USB cable between the PC host and the OpenSDA USB port (J2) on twrk64f120m board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
This demo is an external flash plain load demo, ROM will copy image in external flash to SRAMX to run:
Build the demo to generate a bin file. Note: If need to generate bin file using MCUXpresso IDE, below steps need to be followed: Set in example Properties->C/C++ Build->Settings->Build steps->Post-build steps->Edit enbable arm-none-eabi-objcopy -v -O binary “&{BuildArtifactFileName}” “&{BuildArtifactFileBaseName}.bin”
This plainload example linked the vector table to 0x00000000, but program to external flash 0x10000000.
Program the bin file to external on board flash via SEGGER J-FLASH Lite(V6.22 or higher):
a. Open SEGGER J-FLASH Lite, select device LPC54S018M.
b. Click the ‘Erase Chip’ to erase the extrenal flash.(if can not success, press SW4 button and reset the board, and try to erase again)
c. Select the bin data file, set the ‘.bin/Erase Start’ address to 0x10000000, then click ‘Program Device’ Note: Please use above way to program the binary file built by armgcc tool chain to external flash. For IAR, KEIL, MCUXpresso IDE, you can use the IDE tool to program the external flash.
When the demo runs successfully, the log would be seen on the terminal like:
FATFS example to demonstrate how to use FATFS with SD card.
Please insert a card into board.
Make file system......The time may be long if the card capacity is big.
Create directory......
Create a file in that directory......
Create a directory in that directory......
List the file in that directory......
General file : F_1.DAT.
Directory file : DIR_2.
Write/read file until encounters error......
Write to above created file.
Read from above created file.
Compare the read/write content......
The read/write content is consistent.
Input 'q' to quit read/write.
Input other char to read/write file again.