Hardware requirements
Micro USB cable
LPCXpresso55S06 board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Running the demo
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
The following lines are printed to the serial terminal when the demo program is executed.
Group GPIO input interrupt example
GINT0 and GINT1 events are configured
Press corresponding switches to generate events
“Group GPIO interrupt 1”” is configured to be invoked when both the switches SW1 and SW4 are pressed at the same time. The interrupt callback prints “GINT1 event detected” message on the serial terminal. This example configures “Group GPIO interrupt 0”” to be invoked when SW3 switch is pressed by the user. The interrupt callback prints “GINT0 event detected” message on the serial terminal.