Hardware requirements

  • Mini/micro USB cable

  • LPCXpresso55S16 board

  • Personal Computer

Board settings

The jumper setting: Default jumpers configuration does not work, you will need to add JP20 and JP21 (JP22 optional for ADC use)

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (P6) on the board

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

After the board is flashed the Tera Term will print message on terminal.

Example output:

AES ECB Test pass
AES CBC Test pass
AES CTR Test pass
SHA-1 Test pass
SHA-256 Test pass