Hardware requirements
Mini/micro USB cable
LPCXpresso55s16 board
Personal Computer
Board settings
ADC CH0A input signal J13-3(PIO0_23). The jumper setting: Default jumpers configuration does not work, you will need to add JP20 and JP21 (JP22 optional for ADC use)
Prepare the Demo
Note: MCUXpresso IDE project default debug console is semihost
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the lpadc dma example in the terminal window:
LPADC DMA Example
ADC Full Range: 65536
Please press any key to trigger the conversion.
Adc conversion word : 0x81008BA1
ADC conversion value: 35745
Adc conversion word : 0x81008BE7
ADC conversion value: 35815
Adc conversion word : 0x81008B14
ADC conversion value: 35604