Hardware requirements
Mini/micro USB cable
LPCXpresso55S36 board
Personal Computer
Board settings
(pmux)VREF connect to 1.6V (3.3V * 15 /31). (nmux)J44-21(PIO1_14).
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the terminal like:
CMP polling driver example RED LED turn on.(pmux > nmux). RED LED turn off.(pmux < nmux).