Hardware requirements
Mini/Micro USB cable
LPCXpresso55S36 board
Personal Computer
Board settings
DAC output pin: J12-4
Prepare the Demo
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
A multimeter may be used to measure the DAC output voltage.
Running the demo
OPAMP EXAMPLE!
Please input a value (0 - 4095) for DAC: