Hardware requirements
Micro USB cable
MC56F80000-EVK board
Personal Computer
Board hardware common setting
Power setting:
Connect J8 pin2 and pin3 Connect J6 pin1 and pin2 Connect J5 pin1 and pin2
Reset pin setting:
Connect J11 pin2 and pin3
Debugger setting:
Connect J13 pin 1-2, 3-4, 5-6, 7-8
Board settings
No special settings are required.
Prepare the Demo
Connect USB cable between the host PC and the J12 USB port on the target board. It setups Multilink and COM port in PC device manager.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board with Multilink debug configuration.
Launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows example output of the CRC driver demo in the terminal window:
CRC Peripheral Driver Example.
Test same string base on different CRC protocols.
test string: 123456789
1.CRC-16 CCIT FALSE: 0x29b1
2.CRC-16 KERMIT: 0x2189
3.CRC-16 MAXIM: 0x44c2
4.CRC-32: 0xcbf43926
5.CRC-32 POSIX: 0x765e7680
Test different strings based on CRC-32 POSIX protocol.
1.test string: abcdefgh
CRC-32 POSIX: 0x5024ec61
2.test string: abcd1234
CRC-32 POSIX: 0x3fbda0ab