Hardware requirements
Mini/micro USB cable
MC56F83000 EVK board
Personal Computer
FreeMASTER 2.5 or later installed on PC
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the Debug USB port (JM60 USB) on the target board. Alternatively, use the USB-to-Serial interface at Boot USB port - see main.c for configuration option.
Compile and download the program to the target board.
Running the demo
Run FreeMASTER and use connection wizard to connect at 115200 bps.
Click on “FreeMASTER Demonstration Project (embedded in device)” on the Welcome page.
Read more information about FreeMASTER tool at http://www.nxp.com/freemaster.