Hardware requirements
USB Type-C cable
MCIMX93AUTO-EVK board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW2 to power on the board.
Connect a USB Type-C cable between the host PC and the J26 USB port on the cpu board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
TPM example to simulate a timer
You will see a "-" or "|" in terminal every 1 second:
-|-|-|-|-|-|-|-|-|-|-|-|-|-|-|-|-|-|-|-|-|-|-|-|-|-|-