Hardware requirements
Mini/micro USB cable
MCX-N9XX-EVK board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Note: MCUXpresso IDE project default debug console is semihost
Connect a micro USB cable between the PC host and the MCU-Link USB port (J5) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows example output of the Mailbox interrupt example in the terminal window:
Mailbox interrupt example
Copy CORE1 image to address: 0x2004e000, size: 6940
Write to the secondary core mailbox register: 1
Read value from the primary core mailbox register: 2
Write to the secondary core mailbox register: 3
Read value from the primary core mailbox register: 4
Write to the secondary core mailbox register: 5
Read value from the primary core mailbox register: 6
Write to the secondary core mailbox register: 7
.
.
.
Note: The “Copy CORE1 image to address…” log message is not displayed on the terminal window when MCUXpresso IDE is used. In case of MCUXpresso IDE the secondary core image is copied to the target memory during startup automatically.