Hardware requirements

  • Mini/micro USB cable

  • MCX-N9XX-EVK board

  • Personal Computer

Board settings

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the MCU-Link USB port (J5) on the board

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

Flash driver API tree Demo Application.

Initializing flash driver.
Flash init successfull!.

Config flash memory access time. 

PFlash Information:
kFLASH_PropertyPflashBlockBaseAddr = x
kFLASH_PropertyPflashSectorSize = x
kFLASH_PropertyPflashTotalSize = x
kFLASH_PropertyPflashPageSize = x

Erase a page of flash
Calling FLASH_EraseNonBlocking() API.
Calling FLASH_VerifyErase() API.
Successfully erased page: xx -> xx

Calling FLASH_Program() API.
Calling FLASH_VerifyProgram() API..
Successfully Programmed and Verified Location: xx-> xx

End of PFlash Example!