Hardware requirements
Micro USB cable
RD-RW61X-BGA board
Personal Computer
LCD-PAR-S035 panel
Board settings
Short JP3, JP44, JP50
Wire R624, R625, R626, R627, R629, R630, R631, R616, R662, R663, R664, R665
Connect LCD-PAR-S035 to header J23, J23-1 match LCD J1-1
Set the switch SW1 on LCD-PAR-S035 to 011 (IM[2:0), note the left one is IM[0], right one is IM[2].
Prepare the Demo
Connect a micro USB cable between the PC host and the MCU-Link USB port (J7) on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the example.
Running the demo
If this example runs correctly, the panel shows as the overview description.