Hardware requirements
Micro USB cable
RD-RW61X-BGA board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the MCU-Link USB port (J7) on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the utick example in the terminal window:
Utick example start...
UTICK delay 1 second...
UTICK delay 1 second...
.
.
.