Hardware requirements
Mini USB cable
TWR-MC56F8200 board
Personal Computer
Board hardware common setting
HW reworkd(workaround):
Connect J18(the mini USB port) pin4 and pin5. Note: This is due to HW design error, correct setting should be: J18 pin4 left empty and pin5 connected GND.
Power setting:
Connect J11 pin1 and pin2 Connect J6 pin1 and J7 pin2
UART setting:
Connect J8 pin3 and pin4 Connect J9 pin3 and pin4
Onboard OSJTAG debugger setting:
Connect J20 pin1 and pin2. Leave J17 open. Note: J17 is only used(connected) when firmware update for onboard debugger OSJTAG. Connect J21 pin 1-2, 3-4, 5-6, 7-8, to setup onboard debugger OSJTAG. Note: when use external debugger(connected to J14), leave all J21 pins open
Board settings
No special settings are required.
Prepare the Demo
Connect USB cable between the host PC and the JM60 USB(J18) port on the target board. It setups OSJTAG and COM port in PC device manager.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board with OSJTAG debug configuration.
Launch the debugger in your IDE to begin running the demo.
Running the demo
These instructions are displayed/shown on the terminal window:
FLASH example Start
Flash Information:
Total Program Flash Size: xx KB, Hex: (xx)
Program Flash Sector Size: xx KB, hex: (xx)
...
Flash is xx
Erase a sector of flash
Successfully Erased Sector xx -> xx
Program a buffer to a sector of flash
Successfully Programmed and Verified Location xx -> xx
End of FLASH example