cmsis_dspi_int_b2b_transfer_slave

Overview

The dspi_int_b2b_transfer example shows how to use DSPI CMSIS driver in interrupt way:

In this example , we need two boards, one board used as DSPI master and another board used as DSPI slave. The file ‘dspi_int_b2b_transfer_slave.c’ includes the DSPI slave code. This example uses the transactional API in DSPI driver.

  1. DSPI master send/received data to/from DSPI slave in interrupt .

Supported Boards