cmsis_enet_txrx_transfer
Overview
CMSIS-Driver defines generic peripheral driver interfaces for middleware making it reusable across a wide range of supported microcontroller devices. The API connects microcontroller peripherals with middleware that implements for example communication stacks, file systems, or graphic user interfaces. More information and usage method please refer to http://www.keil.com/pack/doc/cmsis/Driver/html/index.html.
The cmsis_enet_transfer example shows how to use CMSIS ENET driver:
In this example, the ENET transmits 20 number broadcast frames and will print the received frame.