cmsis_pflash
Overview
The CMSIS pflash example shows how to use CMSIS flash driver to operate program flash:
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
PFLASH CMSIS example Start PFlash Information: Total Program Flash Size: xx KB, Hex: (xx) Program Flash Sector Size: xx KB, hex: (xx) Erase a sector of flash Successfully Erased Sector xx -> xx Program a buffer to a sector of flash Successfully Programmed and Verified Location xx -> xx
End of PFLASH CMSIS example