cmsis_i2c_edma_transfer
Overview
CMSIS-Driver defines generic peripheral driver interfaces for middleware making it reusable across a wide range of supported microcontroller devices. The API connects microcontroller peripherals with middleware that implements for example communication stacks, file systems, or graphic user interfaces. More information and usage method please refer to http://www.keil.com/pack/doc/cmsis/Driver/html/index.html.
The cmsis_i2c_edma_transfer example shows how to use I2C cmsis driver in DMA way:
In this example , one i2c instance used as I2C master and another i2c instance used as I2C slave .
I2C master send data to I2C slave with DMA . (I2C Slave using interrupt to receive the data)
I2C master read data from I2C slave with DMA . (I2C Slave using interrupt to send the data)