cmsis_lpspi_int_b2b_transfer_slave
Overview
The lpspi_int_b2b_transfer example shows how to use LPSPI CMSIS driver in interrupt way:
In this example , we need two boards, one board used as LPSPI master and another board used as LPSPI slave. The file ‘cmsis_lpspi_int_b2b_transfer_slave.c’ includes the LPSPI slave code. This example uses the transactional API in LPSPI driver.
LPSPI master send/received data to/from LPSPI slave in interrupt .