slcd_guessnum
Overview
The SLCD number guess demo application demonstrates the use of the SLCD peripheral and driver.
The SLCD number guess demo has two demo displays:
The first demo is a basic SLCD test, where all numbers and icons are shown one by one on the screen.
The second demo is the “Number Guess” game. This demo asks the user to input a number. The demo then provides clues to the user to help the user guess the correct number.
“Great, xxx you has GOT it!” will be shown on the console, and the victory will be displayed on the LCD screen when the user successfully guesses the correct number.