ele_crypto_common

Overview

The ELE Crypto Example project is a demonstration program that uses the MCUX SDK software to perform crypto operations with EdgeLock Enclave (ELE) and usage of its services with direct use of Messaging Unit driver.

Running the demo

Example output on terminal:

EdgeLock Enclave Sub-System crypto example:

****************** Load EdgeLock FW *********************** EdgeLock FW loaded and authenticated successfully.

****************** Compute Hash (SHA256) of massage ******* SUCCESS Computed HASH matches the expected value.

SUCCESS HASH Init done.

SUCCESS HASH Update done.

SUCCESS Computed HASH (Finish) matches the expected value.

****************** Start RNG ****************************** EdgeLock RNG Start success.

EdgeLock RNG ready to use.

****************** Get RNG Random ********************** Get RNG random data successfully. First word: 0xbcd7f0de

End of Example with SUCCESS!!

Supported Boards