Developing a new USB application
The following sections provide information regarding how to develop a new USB application.
Developing a new USB device application
This chapter introduces how to develop a new USB device application. The user needs to use the application interface and the following steps to develop a new application.
Application interfaces
The interface definition between the application and the classes includes the calls shown in the following table:
|API Call|Description| |Class Initialization|This API is used to initialize the class.| |Receive Data|This API is used by the application to receive data from the host system.| |Send Data|This API is used by the application to send data to the host system.| |USB descriptor-related callback|Handles the callback to get the descriptor.| |USB Device call back function|Handles the callback by the class driver to inform the application about various USB bus events.| |USB Class-specific call back function|Handles the specific callback of the class.|
Parent topic:Developing a new USB device application
How to develop a new device application
Perform these steps to develop a new device application:
Create a new application directory under
<install_dir>/boards/<board>/usb_examples/usb_device_<class>_<application>
to locate the application source files and header files. For example,<install_dir>/boards/<board>/usb_examples/usb_device_hid_test.
Copy the following files from the similar existing applications to the application directory that is created in Step 1.
usb_device_descriptor.c usb_device_descriptor.h
The
usb_device_descriptor.c
andusb_device_descriptor.h
files contain the USB descriptors that are dependent on the application and the class driver.Copy the bm directory from the similar existing application directory to the new application directory. Remove the unused project directory from the bm directory. Modify the project directory name to the new application project name. For example, to create
toolchain-IAR, board-frdmk64 class-hid related application
, create the new applicationhid_test
based on a similar existing applicationhid_mouse.
Change
<install_dir>/boards/<board>/usb_examples/usb_device_hid_mouse
to<install_dir>/boards/<board>/usb_examples/usb_device_hid_test
Modify the project file name to the new application project file name, for example, from
dev_hid_mouse_bm.ewp
todev_hid_test_bm.ewp
. Globally replace the existing name to the new project name by editing the project files. Thedev_hid_test_bm.ewp
file includes the new application project setting.Create a new source file to implement the main application functions and callback functions. The name of this file is similar to the new application name, such as
mouse.c
andkeyboard.c
.
The following sections describe the steps to change application files created in the steps above to match the new application.
Changing the usb_device_descriptor.c file
This file contains the class driver interface. It also contains USB standard descriptors such as device descriptor, configuration descriptor, string descriptor, and the other class-specific descriptors that are provided to class driver when required.
The lists below show user-modifiable variable types for an already implemented class driver. The user should also modify the corresponding MACROs defined in the usb_device_descriptor.h file. See the MCUXpresso SDK API Reference Manual (document MCUXSDKAPIRM) for details.
usb_device_endpoint_struct_t;
usb_device_endpoint_list_t;
usb_device_interface_struct_t;
usb_device_interfaces_struct_t;
usb_device_interface_list_t;
usb_device_class_struct_t;
usb_device_class_config_struct_t;
usb_device_class_config_list_struct_t;
This diagram shows the relationship between these items:
|
|
This is the sample code implementation of the endpoint descriptor for the HID class:
/* HID mouse endpoint information */
usb_device_endpoint_struct_t g_UsbDeviceHidMouseEndpoints[USB_HID_MOUSE_ENDPOINT_COUNT] =
{
/* HID mouse interrupt IN pipe */
{
USB_HID_MOUSE_ENDPOINT_IN | (USB_IN << USB_DESCRIPTOR_ENDPOINT_ADDRESS_DIRECTION_SHIFT),
USB_ENDPOINT_INTERRUPT,
FS_HID_MOUSE_INTERRUPT_IN_PACKET_SIZE,
},
};
The endpoint address, transfer type, and max packet size in this variable are defined in the usb_device_descriptor.h file. The user may change these value as required. For example, to implement a CDC class application:
/* Define endpoint for a communication class */
usb_device_endpoint_struct_t g_UsbDeviceCdcVcomCicEndpoints[USB_CDC_VCOM_ENDPOINT_CIC_COUNT] = {
{
USB_CDC_VCOM_INTERRUPT_IN_ENDPOINT | (USB_IN << 7U), USB_ENDPOINT_INTERRUPT,
FS_CDC_VCOM_INTERRUPT_IN_PACKET_SIZE,
},
};
/* Define endpoint for data class */
usb_device_endpoint_struct_t g_UsbDeviceCdcVcomDicEndpoints[USB_CDC_VCOM_ENDPOINT_DIC_COUNT] = {
{
USB_CDC_VCOM_BULK_IN_ENDPOINT | (USB_IN << 7U), USB_ENDPOINT_BULK, FS_CDC_VCOM_BULK_IN_PACKET_SIZE,
},
{
USB_CDC_VCOM_BULK_OUT_ENDPOINT | (USB_OUT << 7U), USB_ENDPOINT_BULK, FS_CDC_VCOM_BULK_OUT_PACKET_SIZE,
}
};
The endpoint count and alternate setting of the interface may differ in various applications. The user may change these values as required. For example, the interface structure of a CDC class application is as follows:
/* Define interface for communication class */
usb_device_interface_struct_t g_UsbDeviceCdcVcomCommunicationInterface[] = {{
1U,
{
USB_CDC_VCOM_ENDPOINT_CIC_COUNT, g_UsbDeviceCdcVcomCicEndpoints,
},
}};
/* Define interface for data class */
usb_device_interface_struct_t g_UsbDeviceCdcVcomDataInterface[] =
{
{
0,
{
USB_CDC_VCOM_ENDPOINT_DIC_COUNT,
g_UsbDeviceCdcVcomDicEndpoints,
},
NULL
}
};
The class code, subclass code, and protocol code may differ in various classes. For example, the usb_device_interfaces_struct of a CDC class is as follows:
/* Define interfaces for the virtual com */
usb_device_interfaces_struct_t g_UsbDeviceCdcVcomInterfaces[USB_CDC_VCOM_INTERFACE_COUNT] = {
{USB_CDC_VCOM_CIC_CLASS, USB_CDC_VCOM_CIC_SUBCLASS, USB_CDC_VCOM_CIC_PROTOCOL, USB_CDC_VCOM_COMM_INTERFACE_INDEX,
g_UsbDeviceCdcVcomCommunicationInterface,
sizeof(g_UsbDeviceCdcVcomCommunicationInterface) / sizeof(usb_device_interfaces_struct_t)},
{USB_CDC_VCOM_DIC_CLASS, USB_CDC_VCOM_DIC_SUBCLASS, USB_CDC_VCOM_DIC_PROTOCOL, USB_CDC_VCOM_DATA_INTERFACE_INDEX,
g_UsbDeviceCdcVcomDataInterface, sizeof(g_UsbDeviceCdcVcomDataInterface) / sizeof(usb_device_interfaces_struct_t)},
};
The interface count may differ in various applications. For example, the usb_device_interface_list of a CDC class application is as follows:
/* Define configurations for virtual com */
usb_device_interface_list_t g_UsbDeviceCdcVcomInterfaceList[USB_DEVICE_CONFIGURATION_COUNT] = {
{
USB_CDC_VCOM_INTERFACE_COUNT, g_UsbDeviceCdcVcomInterfaces,
},
};
The interface list, class type and configuration count may differ in various applications. For example, the usb_device_class_struct of a CDC class application is as follows:
/* Define class information for virtual com */
usb_device_class_struct_t g_UsbDeviceCdcVcomConfig = {
g_UsbDeviceCdcVcomInterfaceList, kUSB_DeviceClassTypeCdc, USB_DEVICE_CONFIGURATION_COUNT,
};
g_UsbDeviceDescriptor
This variable contains the USB Device Descriptor.
Sample code implementation of the device descriptor for the HID class is shown as follows:
uint8_t g_UsbDeviceDescriptor[USB_DESCRIPTOR_LENGTH_DEVICE] = { USB_DESCRIPTOR_LENGTH_DEVICE, /* Size of this descriptor in bytes */ USB_DESCRIPTOR_TYPE_DEVICE, /* DEVICE Descriptor Type */ USB_SHORT_GET_LOW(USB_DEVICE_SPECIFIC_BCD_VERSION), USB_SHORT_GET_HIGH(USB_DEVICE_SPECIFIC_BCD_VERSION),/* USB Specification Release Number in Binary-Coded Decimal (i.e., 2.10 is 210H). */ USB_DEVICE_CLASS, /* Class code (assigned by the USB-IF). */ USB_DEVICE_SUBCLASS, /* Subclass code (assigned by the USB-IF). */ USB_DEVICE_PROTOCOL, /* Protocol code (assigned by the USB-IF). */ USB_CONTROL_MAX_PACKET_SIZE, /* Maximum packet size for endpoint zero (only 8, 16, 32, or 64 are valid) */ 0xA2U, 0x15U, /* Vendor ID (assigned by the USB-IF) */ 0x7CU, 0x00U, /* Product ID (assigned by the manufacturer) */ USB_SHORT_GET_LOW(USB_DEVICE_DEMO_BCD_VERSION), USB_SHORT_GET_HIGH(USB_DEVICE_DEMO_BCD_VERSION),/* Device release number in binary-coded decimal */ 0x01U, /* Index of string descriptor describing manufacturer */ 0x02U, /* Index of string descriptor describing product */ 0x00U, /* Index of string descriptor describing the device serial number */ USB_DEVICE_CONFIGURATION_COUNT, /* Number of possible configurations */ };
The macros in the variable above are defined in the usb_device_descriptor.h file, such as the USB_DEVICE_CLASS, USB_DEVICE_SUBCLASS, and USB_DEVICE_PROTOCOL. Those values may need to be modified as required. The vendor ID and product ID can also be modified.
g_UsbDeviceConfigurationDescriptor
This variable contains the USB Configuration Descriptor.
Sample code implementation of the configuration descriptor for the HID class is providing in the following:
uint8_t g_UsbDeviceConfigurationDescriptor[USB_DESCRIPTOR_LENGTH_CONFIGURATION_ALL] = { USB_DESCRIPTOR_LENGTH_CONFIGURE, /* Size of this descriptor in bytes */ USB_DESCRIPTOR_TYPE_CONFIGURE, /* CONFIGURATION Descriptor Type */ USB_SHORT_GET_LOW(USB_DESCRIPTOR_LENGTH_CONFIGURATION_ALL), USB_SHORT_GET_HIGH(USB_DESCRIPTOR_LENGTH_CONFIGURATION_ALL),/* Total length of data returned for this configuration. */ USB_HID_MOUSE_INTERFACE_COUNT, /* Number of interfaces supported by this configuration */ USB_HID_MOUSE_CONFIGURE_INDEX, /* Value to use as an argument to the SetConfiguration() request to select this configuration */ 0x00U, /* Index of string descriptor describing this configuration */ (USB_DESCRIPTOR_CONFIGURE_ATTRIBUTE_D7_MASK) | (USB_DEVICE_CONFIG_SELF_POWER << USB_DESCRIPTOR_CONFIGURE_ATTRIBUTE_SELF_POWERED_SHIFT) | (USB_DEVICE_CONFIG_REMOTE_WAKEUP << USB_DESCRIPTOR_CONFIGURE_ATTRIBUTE_REMOTE_WAKEUP_SHIFT), /* Configuration characteristics D7: Reserved (set to one) D6: Self-powered D5: Remote Wakeup D4...0: Reserved (reset to zero) */ USB_DEVICE_MAX_POWER, /* Maximum power consumption of the USB * device from the bus in this specific * configuration when the device is fully * operational. Expressed in 2 mA units * (i.e., 50 = 100 mA). */
The macro USB_DESCRIPTOR_LENGTH_CONFIGURATION_ALL, which is defined in the usb_device_descriptor.h, needs to be modified to equal the size of this variable. The interface count and configuration index may differ in various applications. For example, this part of a CDC class application is as shown below:
/* Size of this descriptor in bytes */
USB_DESCRIPTOR_LENGTH_CONFIGURE,
/* CONFIGURATION Descriptor Type */
USB_DESCRIPTOR_TYPE_CONFIGURE,
/* Total length of data returned for this configuration. */
USB_SHORT_GET_LOW(USB_DESCRIPTOR_LENGTH_CONFIGURATION_ALL),
USB_SHORT_GET_HIGH(USB_DESCRIPTOR_LENGTH_CONFIGURATION_ALL),
/* Number of interfaces supported by this configuration */
USB_CDC_VCOM_INTERFACE_COUNT,
/* Value to use as an argument to the SetConfiguration() request to select this configuration */
USB_CDC_VCOM_CONFIGURE_INDEX,
/* Index of string descriptor describing this configuration */
0,
/* Configuration characteristics D7: Reserved (set to one) D6: Self-powered D5: Remote Wakeup D4...0: Reserved
(reset to zero) */
(USB_DESCRIPTOR_CONFIGURE_ATTRIBUTE_D7_MASK) |
(USB_DEVICE_CONFIG_SELF_POWER << USB_DESCRIPTOR_CONFIGURE_ATTRIBUTE_SELF_POWERED_SHIFT) |
(USB_DEVICE_CONFIG_REMOTE_WAKEUP << USB_DESCRIPTOR_CONFIGURE_ATTRIBUTE_REMOTE_WAKEUP_SHIFT),
/* Maximum power consumption of the USB * device from the bus in this specific * configuration when the device is
fully * operational. Expressed in 2 mA units * (i.e., 50 = 100 mA). */
USB_DEVICE_MAX_POWER,
The interface descriptor may differ from various applications. For example, the interface descriptor of a CDC class application would be as shown below.
/* Communication Interface Descriptor */
USB_DESCRIPTOR_LENGTH_INTERFACE, USB_DESCRIPTOR_TYPE_INTERFACE, USB_CDC_VCOM_COMM_INTERFACE_INDEX, 0x00,
USB_CDC_VCOM_ENDPOINT_CIC_COUNT, USB_CDC_VCOM_CIC_CLASS, USB_CDC_VCOM_CIC_SUBCLASS, USB_CDC_VCOM_CIC_PROTOCOL,
0x00, /* Interface Description String Index*/
The class specific descriptor may differ from various applications. For example, the class specific descriptor of a CDC class application would be as shown below.
/* CDC Class-Specific descriptor */
USB_DESCRIPTOR_LENGTH_CDC_HEADER_FUNC, /* Size of this descriptor in bytes */
USB_DESCRIPTOR_TYPE_CDC_CS_INTERFACE, /* CS_INTERFACE Descriptor Type */
HEADER_FUNC_DESC, 0x10,
0x01, /* USB Class Definitions for Communications the Communication specification version 1.10 */
USB_DESCRIPTOR_LENGTH_CDC_CALL_MANAG, /* Size of this descriptor in bytes */
USB_DESCRIPTOR_TYPE_CDC_CS_INTERFACE, /* CS_INTERFACE Descriptor Type */
CALL_MANAGEMENT_FUNC_DESC,
0x01, /*Bit 0: Whether device handle call management itself 1, Bit 1: Whether device can send/receive call
management information over a Data Class Interface 0 */
0x01, /* Indicates multiplexed commands are handled via data interface */
USB_DESCRIPTOR_LENGTH_CDC_ABSTRACT, /* Size of this descriptor in bytes */
USB_DESCRIPTOR_TYPE_CDC_CS_INTERFACE, /* CS_INTERFACE Descriptor Type */
USB_CDC_ABSTRACT_CONTROL_FUNC_DESC,
0x06, /* Bit 0: Whether device supports the request combination of Set_Comm_Feature, Clear_Comm_Feature, and
Get_Comm_Feature 0, Bit 1: Whether device supports the request combination of Set_Line_Coding,
Set_Control_Line_State, Get_Line_Coding, and the notification Serial_State 1, Bit ... */
USB_DESCRIPTOR_LENGTH_CDC_UNION_FUNC, /* Size of this descriptor in bytes */
USB_DESCRIPTOR_TYPE_CDC_CS_INTERFACE, /* CS_INTERFACE Descriptor Type */
USB_CDC_UNION_FUNC_DESC, 0x00, /* The interface number of the Communications or Data Class interface */
0x01, /* Interface number of subordinate interface in the Union */
The endpoint descriptor may differ from various applications. For example, the endpoint descriptor of a CDC class application is as follows:
/*Notification Endpoint descriptor */
USB_DESCRIPTOR_LENGTH_ENDPOINT, USB_DESCRIPTOR_TYPE_ENDPOINT, USB_CDC_VCOM_INTERRUPT_IN_ENDPOINT | (USB_IN << 7U),
USB_ENDPOINT_INTERRUPT, USB_SHORT_GET_LOW(FS_CDC_VCOM_INTERRUPT_IN_PACKET_SIZE),
USB_SHORT_GET_HIGH(FS_CDC_VCOM_INTERRUPT_IN_PACKET_SIZE), FS_CDC_VCOM_INTERRUPT_IN_INTERVAL,
}
String Descriptors
Users can modify string descriptors to customize their product. String descriptors are written in the UNICODE format. An appropriate language identification number is specified in the USB_STR_0. Multiple language support can also be added.
USB_DeviceGetDeviceDescriptor
This interface function is invoked by the application. This call is made when the application receives the kUSB_DeviceEventGetDeviceDescriptor event from the Host. Mandatory descriptors that an application is required to implement are as follows:
Device Descriptor
Configuration Descriptor
Class-Specific Descriptors (For example, for HID class implementation, Report Descriptor, and HID Descriptor) Apart from the mandatory descriptors, an application should also implement various string descriptors as specified by the Device Descriptor and other configuration descriptors.
Sample code for HID class application is as follows:
/* Get device descriptor request */ usb_status_t USB_DeviceGetDeviceDescriptor(usb_device_handle handle, usb_device_get_device_descriptor_struct_t *deviceDescriptor) { deviceDescriptor->buffer = g_UsbDeviceDescriptor; deviceDescriptor->length = USB_DESCRIPTOR_LENGTH_DEVICE; return kStatus_USB_Success; }
The user may assign the appropriate variable of the device descriptor. For example, if the device descriptor variable name is g_UsbDeviceDescriptorUser, the sample code is as follows:
/* Get device descriptor request */
usb_status_t USB_DeviceGetDeviceDescriptor(usb_device_handle handle,
usb_device_get_device_descriptor_struct_t *deviceDescriptor)
{
deviceDescriptor->buffer = g_UsbDeviceDescriptorUser;
deviceDescriptor->length = USB_DESCRIPTOR_LENGTH_DEVICE;
return kStatus_USB_Success;
}
USB_DeviceGetConfigurationDescriptor
This interface function is invoked by the application. This call is made when the application receives the kUSB_DeviceEventGetConfigurationDescriptor event from the Host.
/* Get device configuration descriptor request */ usb_status_t USB_DeviceGetConfigurationDescriptor( usb_device_handle handle, usb_device_get_configuration_descriptor_struct_t *configurationDescriptor) { if (USB_HID_MOUSE_CONFIGURE_INDEX > configurationDescriptor->configuration) { configurationDescriptor->buffer = g_UsbDeviceConfigurationDescriptor; configurationDescriptor->length = USB_DESCRIPTOR_LENGTH_CONFIGURATION_ALL; return kStatus_USB_Success; } return kStatus_USB_InvalidRequest; }
The macro HID_MOUSE_CONFIGURE_INDEX may differ from various applications. For example, the implementation of a CDC class application would be as follows:
usb_status_t USB_DeviceGetConfigurationDescriptor(
usb_device_handle handle, usb_device_get_configuration_descriptor_struct_t *configurationDescriptor)
{
if (USB_CDC_VCOM_CONFIGURE_INDEX > configurationDescriptor->configuration)
{
configurationDescriptor->buffer = g_UsbDeviceConfigurationDescriptor;
configurationDescriptor->length = USB_DESCRIPTOR_LENGTH_CONFIGURATION_ALL;
return kStatus_USB_Success;
}
return kStatus_USB_InvalidRequest;
}
USB_DeviceGetStringDescriptor
This interface function is invoked by the application. This call is made when the application receives the kUSB_DeviceEventGetStringDescriptor event from the Host.
See the usb_device_hid_mouse example for sample code.
USB_DeviceGetHidReportDescriptor
This interface function is invoked by the application. This call is made when the application receives the kUSB_DeviceEventGetHidReportDescriptor event from the Host.
See the usb_device_hid_mouse example for sample code.
USB_DeviceSetSpeed
Because HS and FS descriptors are different, the device descriptors and configurations need to be updated to match the current speed. By default, the device descriptors and configurations are configured using FS parameters for EHCI, KHCI, and other controllers, such as LPC IP3511. When the EHCI is enabled, the application needs to call this function to update the device by using the current speed. The updated information includes the endpoint max packet size, endpoint interval, and so on.
Parent topic:How to develop a new device application
Changing the usb_device_descriptor.h file
This file is mandatory for the application to implement. The usb_device_descriptor.c file includes this file for function prototype definitions. When the user modifies the usb_device_descriptor.c, MACROs in this file should also be modified.
Parent topic:How to develop a new device application
Changing the application file
Main application function
The main application function is provided by two functions: USB_DeviceApplicationInit and APP_task (optional).
The USB_DeviceApplicationInit enables the clock and the USB interrupt and also initialize the specific USB class. See the usb_device_hid_mouse example for the sample code.
USB device call back function
The device callback function handles the USB device-specific requests. See the usb_device_hid_mouse example for the sample code.
USB Class-specific call back function
The class callback function handles the USB class-specific requests. See the usb_device_hid_mouse example for the sample code.
Parent topic:How to develop a new device application
Parent topic:Developing a new USB device application
Parent topic:Developing a new USB application
Developing a new USB host application
Background
In the USB system, the host software controls the bus and talks to the target devices following the rules defined by the specification. A device is represented by a configuration that is a collection of one or more interfaces. Each interface comprises one or more endpoints. Each endpoint is represented as a logical pipe from the application software perspective.
The host application software registers a callback with the USB host stack, which notifies the application about the device attach/detach events and determines whether the device is supported or not. The following figure shows the enumeration and detachment flow.
|
|
The USB host stack is a few lines of code executed before starting communication with the USB device. The examples on the USB stack are written with class driver APIs. Class drivers work with the host API as a supplement to the functionality. They make it easy to achieve the target functionality (see example sources for details) without dealing with the implementation of standard routines. The following code steps are taken inside a host application driver for any specific device.
Parent topic:Developing a new USB host application
How to develop a new host application
Creating a project
Perform the following steps to create a project.
Create a new application directory under
<install_dir>/boards/<board>/usb_examples/usb_host_<class>_<application>
to locate the application source files and header files. For example,<install_dir>/boards/<board>/usb_examples/usb_host_hid_mouse
.Copy the following files from the similar existing applications to the application directory that is created in step 1.
app.c
usb_host_config.h
The app.c file contains the common initialization code for USB host and the usb_host_config.h file contains the configuration MACROs for the USB host.
Copy the bm directory from the similar existing application directory to the new application directory. Remove the unused project directory from the bm directory. Modify the project directory name to the new application project name. For example,
to create toolchain-IAR, board-frdmk64 class-hid related application
, create the new applicationhid_test
based on a similar existing applicationhid_mouse
.Copy
<install_dir>/boards/frdmk64f/usb_examples/usb_host_hid_mouse/bm
to
<install_dir>/boards/frdmk64f/usb_examples/usb_host_hid_test/bm
Modify the project file name to the new application project file name, for example, from
host_hid_mouse_bm.ewp
tohost_hid_test_bm.ewp
. Globally replace the existing name to the new project name by editing the project files. Thehost_hid_test_bm.ewp
file includes the new application project setting.Create a new source file to implement the main application function, application task function, and the callback function. The name of this file is similar to the new application name, such as
host_mouse.c
andhost_keyboard.c
.
The following sections describe the steps to modify application files created in the steps above to match the new application.
Parent topic:How to develop a new host application
Main application function flow
In the main application function, follow these steps:
|
|
Initialize the USB clock.
Call the MCUXpresso SDK API to initialize the KHCI, the EHCI USB clock, or other controller.
Initialize the host controller.
This allows the stack to initialize the necessary memory required to run the stack and register the callback function to the stack.
For example:
status = USB_HostInit(CONTROLLER_ID, &g_HostHandle, USB_HostEvent);
Enable the USB ISR.
Set the USB interrupt priority and enable the USB interrupt.
Initialize the host stack task and application task.
For example (Bare metal):
while (1) { USB_HostTaskFn(g_HostHandle); USB_HostMsdTask(&g_MsdCommandInstance);
Note that in this code, the g_MsdCommandInstance variable contains all states and pointers used by the application to control or operate the device. If implementing the application task as USB_HostHidTestTask and use g_HidTestInstance to maintain the application states, modify the code as follows:
while (1) { USB_HostTaskFn(g_HostHandle); USB_HostHidTestTask(&g_HidTestInstance); }
Parent topic:How to develop a new host application
Event callback function
In the app.c file, there is one USB_HostEvent
function. By default, the function is registered to the host stack when calling the USB_HostInit
. In the USB Host stack, customers do not have to write any enumeration code. When the device is connected to the host controller, the USB Host stack enumerates the device. The device attach/detach events are notified by this callback function.
Application needs to implement one or more functions to correspond to one class process. These application functions are called in the USB_HostEvent
. The device’s configuration handle and interface list are passed to the application through the function so that the application can determine whether the device is supported by this application.
There are four events in the callback: kUSB_HostEventAttach, kUSB_HostEventNotSupported, kUSB_HostEventEnumerationDone, and kUSB_HostEventDetach
.
The events occur as follows:
When one device is attached, host stack notifies
kUSB_HostEventAttach
.The application returns
kStatus_USB_Success
to notify the host stack that the device configuration is supported by this class application, or return thekStatus_USB_NotSupported
to notify the host stack that the device configuration is not supported by this class application.The Host stack continues for enumeration if the device is supported by the application and notifies
kUSB_HostEventEnumerationDone
when the enumeration is done.The Host stack checks the next device’s configuration if the current configuration is not supported by the application.
When the Host stack checks all configurations and all are not supported by the application, it notifies the
kUSB_HostEventNotSupported
.When the device detaches, the Host stack notifies the
kUSB_HostEventDetach
.
This is the sample code for the HID mouse application. The USB_HostHidMouseEvent
function should be called bythe USB_HostEvent
. In this code, the g_HostHidMouse
variable contains all states and pointers used by the application to control or operate the device:
usb_status_t USB_HostHidMouseEvent
(
usb_device_handle deviceHandle,
usb_host_configuration_handle configurationHandle,
uint32_t eventCode
)
{
/* Process the same and supported device's configuration handle */
static usb_host_configuration_handle s_ConfigHandle = NULL;
usb_status_t status = kStatus_USB_Success;
uint8_t id;
usb_host_configuration_t *configuration;
uint8_t interfaceIndex;
usb_host_interface_t *interface;
switch (eventCode)
{
case kUSB_HostEventAttach:
/* judge whether is configurationHandle supported */
configuration = (usb_host_configuration_t *)configurationHandle;
for (interfaceIndex = 0; interfaceIndex < configuration->interfaceCount; ++interfaceIndex)
{
interface = &configuration->interfaceList[interfaceIndex];
id = interface->interfaceDesc->bInterfaceClass;
if (id != USB_HOST_HID_CLASS_CODE)
{
continue;
}
id = interface->interfaceDesc->bInterfaceSubClass;
if ((id != USB_HOST_HID_SUBCLASS_CODE_NONE) && (id != USB_HOST_HID_SUBCLASS_CODE_BOOT))
{
continue;
}
id = interface->interfaceDesc->bInterfaceProtocol;
if (id != USB_HOST_HID_PROTOCOL_MOUSE)
{
continue;
}
else
{
/* the interface is supported by the application */
g_HostHidMouse.deviceHandle = deviceHandle;
g_HostHidMouse.interfaceHandle = interface;
s_ConfigHandle = configurationHandle;
return kStatus_USB_Success;
}
}
status = kStatus_USB_NotSupported;
break;
case kUSB_HostEventNotSupported:
break;
case kUSB_HostEventEnumerationDone:
if (s_ConfigHandle == configurationHandle)
{
if ((g_HostHidMouse.deviceHandle != NULL) && (g_HostHidMouse.interfaceHandle != NULL))
{
/* the device enumeration is done */
if (g_HostHidMouse.deviceState == kStatus_DEV_Idle)
{
g_HostHidMouse.deviceState = kStatus_DEV_Attached;
}
else
{
usb_echo("not idle mouse instance\r\n");
}
}
}
break;
case kUSB_HostEventDetach:
if (s_ConfigHandle == configurationHandle)
{
/* the device is detached */
s_ConfigHandle = NULL;
if (g_HostHidMouse.deviceState != kStatus_DEV_Idle)
{
g_HostHidMouse.deviceState = kStatus_DEV_Detached;
}
}
break;
default:
break;
}
return status;
}
If implementing the callback as USB_HostHidTestEvent
, use g_HidTestInstance
, and support the device that the class code is USB_HOST_HID_TEST_CLASS_CODE, sub-class code is USB_HOST_HID_TEST_SUBCLASS_CODE, and the protocol is USB_HOST_HID_TEST_PROTOCOL. The code can be modified as follows:
usb_status_t USB_HostHidMouseEvent
(
usb_device_handle deviceHandle,
usb_host_configuration_handle configurationHandle,
uint32_t eventCode
)
{
/* Process the same and supported device's configuration handle */
static usb_host_configuration_handle s_ConfigHandle = NULL;
usb_status_t status = kStatus_USB_Success;
uint8_t id;
usb_host_configuration_t *configuration;
uint8_t interfaceIndex;
usb_host_interface_t *interface;
switch (eventCode)
{
case kUSB_HostEventAttach:
/* judge whether is configurationHandle supported */
configuration = (usb_host_configuration_t *)configurationHandle;
for (interfaceIndex = 0; interfaceIndex < configuration->interfaceCount; ++interfaceIndex)
{
interface = &configuration->interfaceList[interfaceIndex];
id = interface->interfaceDesc->bInterfaceClass;
if (id != USB_HOST_HID_TEST_CLASS_CODE)
{
continue;
}
id = interface->interfaceDesc->bInterfaceSubClass;
if (id != USB_HOST_HID_TEST_SUBCLASS_CODE)
{
continue;
}
id = interface->interfaceDesc->bInterfaceProtocol;
if (id != USB_HOST_HID_TEST_PROTOCOL)
{
continue;
}
else
{
/* the interface is supported by the application */
g_HidTestInstance.deviceHandle = deviceHandle;
g_HidTestInstance.interfaceHandle = interface;
s_ConfigHandle = configurationHandle;
return kStatus_USB_Success;
}
}
status = kStatus_USB_NotSupported;
break;
case kUSB_HostEventNotSupported:
break;
case kUSB_HostEventEnumerationDone:
if (s_ConfigHandle == configurationHandle)
{
if ((g_HidTestInstance.deviceHandle != NULL) && (g_HidTestInstance.interfaceHandle != NULL))
{
/* the device enumeration is done */
if (g_HidTestInstance.deviceState == kStatus_DEV_Idle)
{
g_HidTestInstance.deviceState = kStatus_DEV_Attached;
}
else
{
usb_echo("not idle mouse instance\r\n");
}
}
}
break;
case kUSB_HostEventDetach:
if (s_ConfigHandle == configurationHandle)
{
/* the device is detached */
s_ConfigHandle = NULL;
if (g_HidTestInstance.deviceState != kStatus_DEV_Idle)
{
g_HidTestInstance.deviceState = kStatus_DEV_Detached;
}
}
break;
default:
break;
}
return status;
}
Note that the kStatus_DEV_Attached
, kStatus_DEV_Detached
MACROs are defined in the example.
Parent topic:How to develop a new host application
Class initialization
When the supported device is attached, the device’s class needs to be initialized.
For example, the HID mouse initialization flow is as follows:
|
|
Call class initialization function to initialize the class instance.
Call class set interface function to set the class interface
When the set interface callback returns successfully, the application can run.
Parent topic:How to develop a new host application
Sending/Receiving data to/from the device
The transfer flow is as follows:
Call the
USB_hostClassxxx
API to begin the transfer.The transfer result is notified by the callback function that is passed as a parameter.
The HID mouse host uses the following code to receive data from the device:
USB_HostHidRecv(classHandle, mouseBuffer, bufferLength, callbackFunction, callbackParameter);
Parent topic:How to develop a new host application
Parent topic:Developing a new USB host application
Parent topic:Developing a new USB application