Bluetooth LE FSCI Black Box
This section describes the functionality, user interactions, and testing methods for the Bluetooth LE FSCI Black Box demo application.
Description
The Bluetooth LE FSCI Black Box demo application gives access to the Bluetooth LE Host Stack via a serial interface using the FSCI protocol. See the FSCI (Framework Serial Communication Interface) manual for the format of the FSCI commands and a full list of supported commands.
The demo can be used with the Test Tool for Connectivity Products. Command Console application can be downloaded from the NXP website or using a custom application that supports the FSCI protocol and commands.
Parent topic:Bluetooth LE FSCI Black Box
Supported platforms
The following platforms support Bluetooth LE FSCI Black Box application:
KW45B41Z-EVK
K32W148-EVK
FRDM-MCXW71
KW47-EVK
MCXW72-EVK
FRDM-MCXW72
Parent topic:Bluetooth LE FSCI Black Box
Usage with Test Tool for connectivity products
The Bluetooth LE FSCI Black Box demo application is designed to be used via serial interface. This can be done using the TEST Tool for Connectivity Products – Command Console application as described below.
Download the demo application onto a supported board.
Connect the board to a USB port of the PC. The UASB COM port drivers must be installed properly and a COM port corresponding to the board should be available.
Open the Test Tool application and connect to the serial port corresponding to the board on which the Bluetooth LE FSCI Black Box application runs. See Figure 1. The serial communication parameters are: baud rate 115200, 8N1, and no flow control.
Select the appropriate Test Tool XML file from the drop-down list for the release being used and send commands to the application. An example is shown in Figure 2.
Parent topic:Bluetooth LE FSCI Black Box
Parent topic:Bluetooth LE stack and demo applications