Hardware requirements

  • Micro USB cable

  • EVK-MIMX8M Plus board

  • J-Link Debug Probe

  • 12V power supply

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

  1. Connect 12V power supply and J-Link Debug Probe to the board, switch SW3 to power on the board

  2. Connect a USB cable between the host PC and the J23 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, following information can be seen on the terminal:


==FlexCAN loopback functional example -- Start.==

Send message from MB8 to MB9
tx word0 = 0x11223344
tx word1 = 0x55667788

Received message from MB9
rx word0 = 0x11223344
rx word1 = 0x55667788

==FlexCAN loopback functional example -- Finish.==