Hardware requirements
Type-C USB cable
FRDM-MCXA166 board
Personal Computer
Board settings
LPSPI:
       MASTER(SPI0)      connect to        SLAVE(SPI1)
Pin Name   Board Location     Pin Name    Board Location
SOUT       J6-6                SIN       J2-10
SIN        J6-5                SOUT      J2-8
SCK        J6-4                SCK       J2-12
PCS0       J6-3                PCS1      J2-6
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal on PC for MCU-Link serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
LPSPI functional interrupt example start.
This example use one lpspi instance as master and another as slave on one board.
Master uses interrupt way and slave uses interrupt way.
Note that some LPSPI instances interrupt is in INTMUX ,you should set the intmux when you porting this example accordingly
Please make sure you make the correct line connection. Basically, the connection is:
LPSPI_master -- LPSPI_slave
   CLK      --    CLK
   PCS      --    PCS
   SOUT     --    SIN
   SIN      --    SOUT
LPSPI transfer all data matched!
End of example.