Hardware requirements
Type-C USB cable
FRDM-MCXW23 Board
Personal Computer
Board settings
Short J4-5 and J5-1.
Prepare the Demo
Connect a USB cable between the host PC and the FRDM board J10.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
CTimer capture example Rising edge triggered and CTimer capture the edge periodically