Hardware requirements
Type-C USB cable
FRDM-MCXW23 Board
Personal Computer
Board settings
Prepare the Demo
Connect a USB cable between the host PC and the FRDM board J10.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
--- Time out reset test start ---
Watchdog reset occurred
--- Window mode refresh test start---
WDOG has be refreshed!
WDOG has be refreshed!
WDOG has be refreshed!
WDOG has be refreshed!
WDOG has be refreshed!
WDOG has be refreshed!
WDOG has be refreshed!
WDOG has be refreshed!
WDOG has be refreshed!
WDOG has be refreshed!
WDOG has be refreshed!
WDOG has be refreshed!
WDOG has be refreshed!
WDOG has be refreshed!