Hardware requirements
Mini/micro USB cable
Personal Computer
Board settings
Make sure the board is setup to boot from flash.
MCUBoot memory layout
In all cases, the MCUBOOT bootloader reserves 128kB at the beginning of the external flash followed by 4.4MB slots for application. The resulting layout for the monolithic application will be as follows:
Region |
From |
To |
Size |
|---|---|---|---|
MCUboot code |
0x08000000 |
0x0801FFFF |
128kB |
Primary slot |
0x08020000 |
0x0845FFFF |
4352kB |
Secondary slot |
0x08460000 |
0x0889FFFF |
4352kB |
MCUBoot is configured to use its
DIRECT_XIPimage handling strategy together with FlexSPI flash remappingFor testing purposes, the image authentication may be disabled in sblconfig.h by uncommenting the
CONFIG_BOOT_OTA_TESTdefinition so that the following is defined:#define MCUBOOT_NO_SIGN #define CONFIG_BOOT_HASH_NO_SIGN #define CONFIG_BOOT_DIGEST_TYPE_SHA256
Image signing example
imgtool sign --key sign-rsa2048-priv.pem
--align 4
--version 1.1
--slot-size 0x440000
--header-size 0x400
--pad-header
ota_mcuboot_basic.bin
ota_mcuboot_basic.SIGNED.bin
Note that for the first image flashed manually together with the bootloader
additional imgtool options --pad and --confirm must be used. Otherwise
the bootloader would reject the image for missing data in the trailer area.