Changelog Multicore Manager

All notable changes to this project will be documented in this file.

The format is based on Keep a Changelog, and this project adheres to Semantic Versioning.

[4.1.7]

Fixed

  • mcmgr_stop_core_internal() function now returns kStatus_MCMGR_NotImplemented status code instead
    of kStatus_MCMGR_Success when device does not support stop of secondary core.
    Ports affected: kw32w1, kw45b41, kw45b42, mcxw716, mcxw727.

[v4.1.6]

Added

  • Multicore Manager moved to standalone repository.

  • Add porting layers for imxrt700, mcmxw727, kw47b42.

  • New MCMGR_ProcessDeferredRxIsr() API added.

[v4.1.5]

Added

  • Add notification into MCMGR_EarlyInit and mcmgr_early_init_internal functions to avoid using uninitialized data in their implementations.

[v4.1.4]

Fixed

  • Avoid calling tx isr callbacks when respective Messaging Unit Transmit Interrupt Enable flag is not set in the CR/TCR register.

  • Messaging Unit RX and status registers are cleared after the initialization.

[v4.1.3]

Added

  • Add porting layers for imxrt1180.

Fixed

  • mu_isr() updated to avoid calling tx isr callbacks when respective Transmit Interrupt Enable flag is not set in the CR/TCR register.

  • mcmgr_mu_internal.c code adaptation to new supported SoCs.

[v4.1.2]

Fixed

  • Update mcmgr_stop_core_internal() implementations to set core state to kMCMGR_ResetCoreState.

[v4.1.0]

Fixed

  • Code adjustments to address MISRA C-2012 Rules

[v4.0.3]

Fixed

  • Documentation updated to describe handshaking in a graphic form.

  • Minor code adjustments based on static analysis tool findings

[v4.0.2]

Fixed

  • Align porting layers to the updated MCUXpressoSDK feature files.

[v4.0.1]

Fixed

  • Code formatting, removed unused code

[v4.0.0]

Added

  • Add new MCMGR_TriggerEventForce() API.

[v3.0.0]

Removed

  • Removed MCMGR_LoadApp(), MCMGR_MapAddress() and MCMGR_SignalReady()

Modified

  • Modified MCMGR_GetStartupData()

Added

  • Added MCMGR_EarlyInit(), MCMGR_RegisterEvent() and MCMGR_TriggerEvent()

  • Added the ability for remote core monitoring and event handling

[v2.0.1]

Fixed

  • Updated to be Misra compliant.

[v2.0.0]

Added

  • Support for lpcxpresso54114 board.

[v1.1.0]

Fixed

  • Ported to KSDK 2.0.0.

[v1.0.0]

Added

  • Initial release.