BDB_vOutOfBandCommissionGetData
void BDB_vOutOfBandCommissionGetData(
BDB_tsOobReadDataToAuthenticate
*psReturnedCommissioningData);
Description
This function is used to obtain locally stored commissioning data. The obtained data is received in a structure described in BDB_tsOobReadDataToAuthenticate and includes the network key. The data is then passed to higher layers which may encrypt it before sending it by out-of-band means to the other device involved in the commissioning.
A similar set of data but with the network key encrypted can be obtained using the function BDB_eOutOfBandCommissionGetDataEncrypted().
For an overview of out-of-band commissioning, refer to Out-Of-Band Commissioning.
Parameters
psReturnedCommissioningData: Pointer to a structure to receive the obtained commissioning data (see BDB_tsOobReadDataToAuthenticate)
Returns
None
Parent topic:Functions