Compile-time options
Before a ZigBee 3.0 application is built, configure compile-time options in the header file zcl_options.h for the application.
Note:
Cluster-specific compile-time options are detailed in the cluster descriptions in the ZCL User Guide (JNUG3132).
In addition, set compile-time options for the ZigBee Base Device in the file bdb_options.h - see Section 2.10.
Number of Endpoints
An application must specify the highest numbered endpoint used by it - for example:
#define BDB_FB_NUMBER_OF_ENDPOINTS3
Normally, the endpoints starting at endpoint 1 are for application use, so the above case uses endpoints 1 to 3. It is possible, however, to use the lower numbered endpoints for non-application purposes, for example, to run other protocols on endpoints 1 and 2, and the application on endpoint 3. With BDB_FB_NUMBER_OF_ENDPOINTS
set to 3, some storage is statically allocated for endpoints 1 and 2 but never used. Note that this define applies only to local endpoints - the application can refer to remote endpoints with numbers beyond the locally defined value of BDB_FB_NUMBER_OF_ENDPOINTS
.
Manufacturer Code
The ZCL allows a manufacturer code to define devices developed by a certain manufacturer. The value allocated to a manufacturer by the ZigBee Alliance is a 16-bit and is set as follows:
#define ZCL_MANUFACTURER_CODE 0x1037
The above example sets the manufacturer code to the default value of 0x1037 (which belongs to NXP) but manufacturers should set their own allocated value.
Enabled Clusters
Enable all the required clusters in the options header file. For example, an application for an On/Off Light device that uses all the possible clusters requires the following definitions:
#define CLD_BASIC
#define CLD_IDENTIFY
#define CLD_GROUPS
#define CLD_SCENES
#define CLD_ONOFF
Server and Client options
Many clusters have options that indicate whether the cluster acts as a server or a client on the local device. If the cluster is enabled using one of the above definitions, define the server/client status of the cluster. For example, to employ the Groups cluster as a server, include the following in the header file:
#define GROUPS_SERVER
Support for attribute Read/Write
Compile read/write access to cluster attributes into the application explicitly. Separately enable the server and client sides of a cluster using the following macros in the options header file:
#define ZCL_ATTRIBUTE_READ_SERVER_SUPPORTED
#define ZCL_ATTRIBUTE_READ_CLIENT_SUPPORTED
#define ZCL_ATTRIBUTE_WRITE_SERVER_SUPPORTED
#define ZCL_ATTRIBUTE_WRITE_CLIENT_SUPPORTED
Each of the above definitions applies to all clusters used in the application.
Optional attributes
Many clusters have optional attributes that may enable at compile time via the options header file - for example, the Basic cluster ‘application version
’ attribute is enabled as follows:
#define CLD_BAS_ATTR_APPLICATION_VERSION
Parent topic:Introduction