Supported clusters

The clusters used by the On/Off Light device are listed in the table below.

Table 14.  Clusters for On/Off Light

Server (Input) side

Client (Output) side

Mandatory

Basic

Identify

On/Off

Scenes

Groups

Optional

Level control

OTA upgrade

Touchlink commissioning

Occupancy sensing

The mandatory attributes within each cluster for this device type are indicated in the ZigBee Lighting and Occupancy Device Specification (15-0014-01).

Parent topic:On/Off light