Examples

The table below lists the example applications provided.

Application

Device type

Coordinator

Coordinator/Trust center

Router

Router

End Device RX On

End Device (Non-sleeping)

End Device RX Off when Idle

End Device (Sleeping)

The examples are provided as part of the wireless examples for ZigBee. The binaries generated by these examples are targeted to run on the K32W148-EVK board, FRDM-MCXW71 board, MCX-W72-EVK, RD-RW612-BGA, and FRDM-RW612 boards.

Note: The RW612 platform does not support the RX OFF Application use case currently.

K32W148-EVK board

The K32W148-EVK board is used for the ZigBee examples described in this document. The important LEDs and user control buttons are highlighted, as shown in the figure below.

Parent topic:Examples

FRDM-MCXW7x board

The FRDM-MCXW7x board is used for the ZigBee examples described in this document. The important LEDs and user control buttons are highlighted, as shown in the figure, FRDM-MCXW7x board below.

Parent topic:Examples

FRDM-MCXW71 / FRDM-MCXW72 board

The FRDM-MCXW71 or the FRDM-MCXW72 board can be used for the ZigBee examples described in this document. The important LEDs and user control buttons are highlighted, as shown in the figure below.

Parent topic:Examples

RD-RW612-BGA board

The FRDM-RW612 board can be used for the ZigBee examples described in this document. The important LEDs and user control buttons are highlighted, as shown in the figure, RD-RW612-BGA board below.

Parent topic:Examples

FRDM-RW612 board

The FRDM-RW612 board is used for the ZigBee examples described in this document. The important LEDs and user control buttons are highlighted, as shown in the figure, FRDM-RW612 board below.

Parent topic:Examples

MCX-W72-EVK board

The MCX-W72-EVK board can be used for the ZigBee examples described in this document. The board is shown in the figure below.

MCX_W72_EVK

Parent topic:Examples