Overview

This document applies to the K32W1/MCXW71/MCXW72/RW612 device ZigBee 3.x wireless microcontrollers, referred to as ZigBee devices throughout this document.

This document provides details of the ZigBee example applications. These examples demonstrate the features and operation of the base device in a ZigBee 3.x network that uses NXP microcontrollers from the K32W1/MCXW71/MCXW72/RW612 families. The examples can be a starting point for developing real-world devices.